This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92513: Differences between TPS92512 and TPS92513

Part Number: TPS92513
Other Parts Discussed in Thread: TPS92512,

Hello,

I am confirming about the difference between TPS92512 and TPS92513.
There seem to be two differences.
The first seems to be the difference in Iout. The difference between 1.5A and 2.5A.
The second is the content shown below.
There is a sense of incongruity that the description is different for MIN and MAX of Falling threshold.
Is this content correct?
Also, please let me know if there are any other differences between both devices.

Best regards,