Other Parts Discussed in Thread: BQ24630,
Hi,
First of all, I have been checking the forums for similar issues, especially on the bq24630 but don't think they are completely similar to my case.
We have been designing chargers based on the bq24618 with no issues. So far we produced a few hundreds that have been operational for a few years (CHGV6).
Now we started designing a version with USB C and tried to increase the power to 5A. To do so, we had an iteration (V8) where we tested both 2xGaN and newer MOSFETs in parallel to test their efficiency (only testing either GaN or MOSFETs). You can also see attached the V8 schematic.
Wrt GaN we followed some recommendations that we have seen from different webinars as GaN have different driver requisites. When we tested the GaN option we suddenly started seeing the issue where STAT1 LED turned on without the battery being connected and we blamed it to some incompatibility issues with driving them.
Then we removed the GaN and added the MOSFETs as seen on CHGV8 production schematics. Everything has been working fine for months, charging batteries without issues. However, last week they suddenly started having the same issues, where STAT1 turns on with no battery connected. We checked waveforms on PH, HDRV, LDRV, REGN and BSTS, attached too.
I replaced the BQ24618 chip on one of the failing chargers and then it worked fine again. Waveforms look good and almost identically as CHGV6. My feeling is that even though we do not connect the GaN Fets, the PH area could be too big in the layout and could mess something up after some time. To me it looks like a layout issue that could damage the bq24618 somehow but would like to confirm that there are no other issues on the schematics (regarding the CHGV8 production variant).
Thanks for your help