Hi Team,
a customer would like to confirm the following:
TLV74033PDQNR: they would like to use the 3.3V output version and we will use it with input voltages below 3.3V so to have an output voltage following the input with a difference of the dropout voltage: Vout = Vin-Vdropout.
Could you please verify if this is possible ?
The goal is to protect a power section from overvoltage (max 3,3V)and overcurrent (about 50mA).
Vin min is 2.5V.
BR,
Stefan