Hello,
Are the Gerber files (or PDF's of them) and the BOM available for the BQ24630EVM LiFePO4 charger circuit?
I have designed a PCB with this chip but I can only get 80% effectiveness on my charger - this is a problem because the switching losses heats up the circuitry too much.
I have designed my circuit exactly according to the development kit - so it must be the board layout.
Can you tell me if it is possible at all to have a good circuit using only a 2 layer PCB?
If you can maybe send me the BQ24630EVM Gerbers so I can use this as an input to help me with the layout
Thanks!
Pieter