I have a few questions/comments on the BQ24035 part that I plan to use. I assume it applies to the entire family.
1) I have mobile computer design where I would like to have a temperature monitoring chip (TI TMP300) to shut down all power to the system with a temperature fault - in my case either AC Adapter, USB or Battery. The over temperature may be due to high ambient temperature or failure of a component that causes overheating. Because of the possibilitiy of component failure (our downstream power supply chip, for example) I can't depend on the processor to decide to shut the system down, instead I need a HW over-ride. Your CE signal input looks close, however still allows the battery to supply power to the system.
- Is there anyway (tricks?) to shut off all power (AC, USB and BAT) to OUT without significant external components?
2) As a future design suggestion:
- It would be very nice to have the battery charge termination point be pin selectable between 4.1 and 4.2V. 4.2V tends to be more industry standard providing additional capacity, but with 4.1V providing significantly increased battery life. Some of my customers would prefer the latter as a tradeoff.
- CE- why is it setup as active high enable? Unless I am doing something wrong it seems much simpler to be active low. Active High makes the circuit design much more complicated because of the input voltage domains (up to 18V) and CE is limited to 7V max. And you have to develop your own high voltage from the AC/USB voltages to provide the active high signal since I can't depend on any supply being present (even the battery).
Thanks for your help,
Bob