This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV755P: Using TLV755P and LP5912 in the same layout

Part Number: TLV755P

Hello,

I am considering using the TLV75533PDRVR and LP5912-3.3DRVR in the same layout.
This is in response to the recent difficulty in obtaining parts.
The packages are the same, and the pinouts are generally compatible.
Can both devices work with the layout shown in the attached image?
In this layout, 3 pin (GND) of the TLV75533PDRVR is not connected, but the datasheet says that Thermal Pad is internally connected to GND, so I think the GND of this device is connected.
In addition, I think that the thermal characteristics will deteriorate because the 3 pin is not connected.

Best regards,