This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM63606: Can TPSM63606 support output 1.8V@6A with 12V input?

Part Number: TPSM63606
Other Parts Discussed in Thread: LM63460-Q1

Hi experts:

Can TPSM63606 support output 1.8V@6A with 12V input?

I am searching for a solution to regulate 12V input to the output 1.8V@6A, 2.5V@6A, 3.3V@6A, 5V@6A, 7.5V@6A, 8V@6A, 10V@6A.

Can TPSM63606 work for this?

Thanks,

Marsh