Dear experts,
Could I ask what will happend on the Vout if the Vin equal to 5V for the TPS7A4101 with feedback resistor 480K (To Vout) and 20Kohm (to GND)?
Thanks!
Dylan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear experts,
Could I ask what will happend on the Vout if the Vin equal to 5V for the TPS7A4101 with feedback resistor 480K (To Vout) and 20Kohm (to GND)?
Thanks!
Dylan
Hi Dylan,
With an Rbottom of 20k and an Rtop of 480K, you are setting the output to 29.325V
Vout ~ Vref(1+Rtop/Rbot)
29.325V = 1.173V (1 + 480K/20K)
This means that if your VIN is 5V, you will be pushing the device into dropout, losing the PSRR, noise and transient performance of the LDO.
However, as you noted, VIN min is 7V, This means that you cannot expect full datasheet performance. I tested a similar device and the device functioned down to below 4V, so with a 5V input it should still work in dropout operation.
Regards,
John
Hi Jonathan,
Really appreciated for your strong support! Could I check with you what will be the output voltage if I have Vin 5V and setting the output to 4V via the feedback resistor Rtop and Rbottom?
Thanks!
Dylan
Hi Dylan,
Dropout is heavily dependent upon temperature and load current for this device. However, at 25C even at full load, the device should regulate to 4V.
In the worst case, VOUT in dropout would be at 3.7V.
Regards,
John