This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62871-Q1: product schedule

Part Number: TPS62871-Q1

Hi Team,

My customer would like to use our TPS62871-Q1 in their new project, they don't need I2C so target to 9A --> TPS62871N1QWRXSRQ1 .

But at tis moment,  TPS62871N1QWRXSRQ1 can't be found in the Orderable Device table, customer need those information to create our solution into their pool first.

So, may I know how is the TPS62871N1QWRXSRQ1 sample/RTM schedule ?

If customer need to create it first, is it possible to provide a modified datasheet and write TPS62871N1QWRXSRQ1 into device table for customer used first ?

If not, any advise for this scenario? Such like implemented another Orderable part first, then transfer to  TPS62871N1QWRXSRQ1 once it ready? If so, which part is more suitable?

They need a 0.8V output part, and plan to stack two in used.

 

Thanks!
Kai