Other Parts Discussed in Thread: CSD17578Q3A, CSD18511Q5A
Hi,
I have designed a custom charger based on bq25720. I need help regarding selection of inductor and 4 switching N-channel MOSFET (Q1, Q2,Q3,Q4).
I have used BMRA000606302R2MA1 in place of BMRHDY1010302R2MA1 ( as suggested in bq25720 EVM board).
and SIRA84BDP-T1-GE3 as 4 switching MOSFET in place of CSD17578Q3A (as suggested in bq25720 EVM board).
Though I have used these components after comparing the spec with the one used in EVM board but I guess these selection might not be correct
as while charging at 4 amp temperature of Mosfet Q1 & Q2, Inductor and nearby PCB area is increasing upto 60-65 degree celsius.
Though charging is happening but the these components are becoming very hot. If I charge with the bq25720 based EVM board temperature rises near to 45 degree celsius only and that too of inductor only.
Note: My PCB board is of 4 layer and I have tried to follow the guidelines as per EVM board.
I am using 24V, 2A power adapter.
I have attached the image of arrangement of MOSFET and Inductor in the PCB.