Other Parts Discussed in Thread: TPS62824A
Hi Experts,
Seeking your assistance on this query:
I am working on a new design and I'm hoping to use certain TI parts.
I'd like to use level translator LSF0108PWR to translate between 3.3 V & 1.8 V, and I'd also like to generate the 1.8 V supply using the TPS62202DBVR DC-DC converter.
Regarding the LSF family of translators, the TI video tutorial linked below (2:16 mark) says that, "It is very important to note that current will be flowing into the A-side (i.e. 1.8 V) supply during normal operation, and not all voltage sources can sink current. So be sure that your design can handle this current."
Question:
Can the 1.8 V regulator handle this current?
https://training.ti.com/tlm-lsf-bias?context=1134826-1139264-1134790
Regards,
Archie A.