This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62202: Can it handle reverse current generated by LSF0108PWR?

Genius 14819 points
Part Number: TPS62202
Other Parts Discussed in Thread: TPS62824A

Hi Experts,

Seeking your assistance on this query:

I am working on a new design and I'm hoping to use certain TI parts. 

I'd like to use level translator LSF0108PWR to translate between 3.3 V & 1.8 V, and I'd also like to generate the 1.8 V supply using the TPS62202DBVR DC-DC converter.

Regarding the LSF family of translators, the TI video tutorial linked below (2:16 mark) says that, "It is very important to note that current will be flowing into the A-side (i.e. 1.8 V) supply during normal operation, and not all voltage sources can sink current.  So be sure that your design can handle this current."

Question:
Can the 1.8 V regulator handle this current? 
https://training.ti.com/tlm-lsf-bias?context=1134826-1139264-1134790

Regards,
Archie A.

  • Hi Archie,

    When you want to sink current into the supply, it is required to choose one of our converters that can operate in FPWM mode and has a negative current limit feature. The TPS62202 doesn't have both features.

    You can check one of our newer devices TPS62824A which operates only in FPWM mode and has a negative current limit spec.

    Best regards,

    Varun