This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM76005-Q1: Tj calculation questions

Part Number: LM76005-Q1

Hi team,

My cusotmer would like to get details on LM76005-Q1 Tj calculation,

Power supply spec:

  • VIN: 16~36V
  • VOUT: 14V/3.5A
  • TA max: 85C

From Webench report, below is calculation result, with ICThetaJA Effective=16.0degC/W.

WBDesign455.pdf

While in datasheet, R thetaJA is also listed, which is 29.6degC/W.

Questions:

1. Can you clarify which thermal resistance can be taken in Tj calculation? Since LM76005-Q1 has thermal pad, in my understanding, R junction to board should be taken, it is 9.1degC/W.

2. For this LM76005-Q1 application, can you provide a Tj calculation result at TA=85C?

Thanks.

Johnny