Other Parts Discussed in Thread: PMP10749,
Hi! I need to design a boost convert the specs with
Application Field : Cold Crank (start stop)
Required Specs for the application : In case of cold crank, the input voltage can drop to 3 volts.So 3 volt and higher input voltage value is required in accordance with this situation.
Vout: 10V output and up to 20A.
I'm trying to create a boost converter with the requirements I mentioned above. I realized that the boost converter in the design of the pmp10749 fits my requirements, However, its 10Amp output is insufficient, so I need a dual phase design. However, I don't know exactly what changes I need to make. How should I connect the syncout pin? ? Do I need to make any changes to the compensation elements? Do I need a change in the capacitor connected to the bst pin?
or other elements ?