I designed a board with 2x DCV010512D to generate +24V and -24V. For the +24V, no pb it works fine.
But for the -24V, I mesured ~-4V:
I connected the input on 0/+5V.
The +Vout is used as ground reference and -Vout as -24V.
I loaded the outputs with 1uF capacitor and 10kohm resitor between 0V and +Vout pins and also between 0V and -Vout.
I connected Sync_in pin of the 2 chip as is discribed in the datasheet (I tried also to disconnected it with the same behavior).
Someone can help me, please?