This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS3702-Q1: the (VIT–) and (VIT+)

Part Number: TPS3702-Q1

Hi  team,

I would like to confirm whether the (VIT –) and (VIT+) error is chip-driven or VDD-related? thanks 

for example ,when i set Vdd=3.3V, 3.3V itself has errors maybe it is 3.2V actually , so in this situation, worst case: VIT –=3.463V and VIT+=3.139V?