Other Parts Discussed in Thread: BQSTUDIO, BQ25713
Hi
The customer design with BQ25723, they designed the board and test it.
Without battery the adapter power the system, it works normal.
Without adapter the battery power the system, it works normal.
After the battery is discharged to 9.6 V, then connect the adapter and battery at the same time. The adapter did not charge the battery.
They used the default value and did not use the BQSTUDIO.
Attached the schematic for your reference.
BQ25723-Mainboard_V1.0_20221008.pdfBQ25723验证板.rar
Why could not charge when the adapter plug in?
Thanks
Star