This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLVM13660: Change R_FBB value

Part Number: TLVM13660

Hi teams,

When we would like to create 5V output voltage from 24V input voltage, The recommended R_FBB value is 10kohm, so R_FBT becomes 40kohm based on the equation (1) on the datasheet.

Is it possible to let R_FBB value 3kohm?

What is the recommended resistor range of R_FBB?

Best regards,

Shunsuke Yamamoto