This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC2894: Output no signal

Part Number: UCC2894

Hello,

I am trying to get ucc2894 working,

but output always no signal,

the IC get VDD is 13.5V, Vref 5V, LineOV less than 1.27, LineUV greater than 1.27V,

the dirve signal (FB) give 4V, CS connect to GND, 

is there other condition I need to consider or how can I test IC can fuction normally?

Thanks for answering.