I have a design where I'd like to have a second (5V) power supply in parallel with the output of a boost converter (1.2V NiMH to 3.3V). The goal is to have either power source feed the device. Will the TPS61261 converter be harmed by backfeeding with 5V from USB? How about if I reduce the 5V to something slightly lower, say 4.5V, so it is well below the maximum voltage rating for all pins?
If this boost converter isn't the best choice for this application, could you suggest one that is? Or there a better best practice for this sort of dual-supply application? I'd rather not have to have a Schottky diode on the output of the boost converter because of the voltage drop.
Thanks!