Other Parts Discussed in Thread: UC3879
Hi Team,
I understand UC2879 is rated for operating ambient temperature of -40°C to 85°C. and UC3879 is rated for operating ambient temperature of 0°C to 70°C. when I look at the junction temperature in the datasheet, it is -55 to 150 degree Celsius for both. May I confirm that this is right information?
Thanks!
Best Regards,
Ernest