I am using the WEBENCH Power designer to design a power supply using the LM25118 buck-boost controller.
My input conditions are Vin min=9V, Vin max=32V, Vout=15V and Iout= 6.7A, ambient temp= 85 Deg C
I would like to use a fsw of 301 kHz, when I put those conditions in the simulator I get an error saying OpVal table param temperature> 150 Deg C. I would like to understand what is causing this error and what the parameter OpVal temp means.