Hi team,
My customer is using TPS54325 and have a question with it.
In the datasheet 8.3.2 "Power Good", it says:
" R_PG resister value ,which is connected between PG and VREG5, is required from 20 kΩ to 150 kΩ"
But currently, my customer is not putting this resister.
So my questions is,
What would happen if they don't put that R_PG?
i know that it is required, so I will ask the customer to install it.
But I would like to know the reason why it is needed, to explain it to the customer.
Regards,
Ohashi