This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3150: EMC conducted emission support

Part Number: LM3150

hi team:

 my customer uses LM3150 and find some CE issue during tests, here attached some modifications but does not work, can you help to review this SCH and LAYOUT? tks !

 LM3150 CE issue.docx

LM3150_design_WL.pdf

LM3150_WL.dwg

sch.jfif

  • Hello Allen,

    Need to place capacitance on the left side of the input inductor, L7, not the right side.  Noise source you are filtering is on the right of the input inductor.  Also, I don't see any input filter damping. please refer to the document below.  the damping capacitor needs to be placed on the right side of the inductor L7.

    Input Filter Design for Switching Power Supplies (ti.com)

    Hope this helps.

    David.

  • Hi David:

     tks for your comments.

     As I see ,If the input circuit has a probability of causing CE problems. Does it means i can short circuit the L7 and connect the DC power supply like battery to verify?

     BTW, is there any layout recommendation? I see the spec highlight SGND need a single trace to PGND, but i did not see the layout recommendation chapter and EVM have these design input. 

     tks for your reply too.

  • Hello Allen,

    You could short out L7 and the emissions will get worse, alternatively you can place a capacitor left side of L7 and observe that various difference values of capacitance will give you various degrees of attenuation in the EMC plot.

    Regarding layout guidelines, there are some in the datasheet.  To answer your question about SGND specifically, yes, suggest tying ground side of all small signal components to an SGND polygon pour and tying the polygon pour back to SGND pin.  Then tie the SGND pin to the DAP of the device.  PGND will have its own polygon pour that is tied back to PGND pin and the PGND pin is connected to the DAP also.  You can place multiple Vias near the SGND, PGND pins and place a few on the DAP.  Vias will be tied to a solid GND layer directly beneath the top layer that the device and power stage are mounted on.

    Please see rough draft of a complete layout/floorplan below, for the LM3150.  hope this helps.

    David.

  • Hi David:

     Tks for your quick feedback.

     Regarding short circuit the L7, what i means is i use a DC power and without inductor, meanwhile there is no frequency of the input section..  but why will cause the emissions will get worse? hope you can share your opinions. tks!

  • Hello Allen,

    If you do emissions testing without L7, the EMI will be worse, suggest using L7 with the recommendations given above.  Thanks.

    David.