Greetings,
I designed the LM5157 circuit according to its eval board. Input voltage is regulated 5V and output is 12V 1 - 1.2 A.
I made some changes on some of the components. Red text near that component is eval board values, so
- Are new resistor values okay for UVLO?
- I won't use PGOOD can i leave this pin floating?
- In eval board C65’s voltage rating is 100V. Can I use a 50V voltage rating 0402 capacitor?
- In eval board C64’s voltage rating is 16V. Can I use a 10V voltage rating capacitor?
- For the L20 inductor can I use 2.2uH instead of 1.5uH (part number of inductor : SRP1265A-2R2M)
- I selected new resistors for FB. Are FB resistors suitable?