Other Parts Discussed in Thread: LM10011, LM10010
Hi,
I would like to use a TPS40345 buck controller to deliver between 1.12V (5W) and 1.5V (9W) to a 0.6 ohm load.
The buck's high side is connected to a 3.7V battery, the TPS 40345 is powered via a 3.3V VDD.
By connecting the FB pin to a DAC, is it possible to control the TPS 40345's output by changing the DAC output ?