This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5030: Push-pull PS problem

Part Number: LM5030

Dear mr.

I have a problem with bring up of PS , see sch.

Spec. Vin=17-27V, Vout=300V, Pout =400W

Voltage feedback is disconnected by removing R259 for simplification

I'm waiting to see  about 50% PWM of MOSFET's control.

But instead I see :GREEN- current U29.8, BLUE & YELLOW is outputs U29.5 and U29.6

Every 200uS packets

After zoom

I see numbers interleaved pulses(with period about 4us, like designed, but small PWM-not 50% ) to gates of power MOSFET

and after I see two not interleaved pulses (at about same time), it produce big current and after about 200us it round robin.  

I replace U29, but it still same result .

Same result with/without light load(1.5kOhm)

Please help.