Hi
I am using the TI TPS6598x Host Interface Tool to execute the DBfg function (clearing the Dead battery flag of the TPS65982 PD Controller).
I used a sniffer to capture the I2C communication between the Host Interface Tool and TPS65982.
Can anyone advise why does it need to read the data in register 0x09 (Data1)? Thanks.
I2C Activity | Description | Function |
write to 0x27 ack data: 0x03 | Read 4 btyes of data from reg 0x03 (Mode) | A P P <SP> The PD Controller is fully functioning in the application firmware. |
read to 0x27 ack data: 0x04 0x41 0x50 0x50 0x20 | Data = 41 50 50 20 (hex) | |
write to 0x27 ack data: 0x08 0x04 0x44 0x42 0x66 0x67 | Write 4 bytes of data to reg ox08 (Cmd1): 44 42 66 67 | Execute function: DBfg |
write to 0x27 ack data: 0x03 | Read 4 btyes of data from reg 0x03 (Mode) | A P P <SP> |
read to 0x27 ack data: 0x04 0x41 0x50 0x50 0x20 | Data = 41 50 50 20 (hex) | |
write to 0x27 ack data: 0x08 | Read 4 btyes of data from reg 0x08 (Cmd1) | The command DBfg is successfully processed. |
read to 0x27 ack data: 0x04 0x00 0x00 0x00 0x00 | Data = 00 00 00 00 (hex) | |
write to 0x27 ack data: 0x03 | Read 4 btyes of data from reg 0x03 (Mode) | A P P <SP> |
read to 0x27 ack data: 0x04 0x41 0x50 0x50 0x20 | Data = 41 50 50 20 (hex) | |
write to 0x27 ack data: 0x09 | Read 64 btyes of data from reg 0x09 (Data1) | ??? |
read to 0x27 ack data: 0x40 0x00 | Data = 00 ……. | |
write to 0x27 ack data: 0x03 | Read 4 btyes of data from reg 0x03 (Mode) | A P P <SP> |
read to 0x27 ack data: 0x04 0x41 0x50 0x50 0x20 | Data = 41 50 50 20 (hex) | |
write to 0x27 ack data: 0x03 | Read 4 btyes of data from reg 0x03 (Mode) | A P P <SP> |
read to 0x27 ack data: 0x04 0x41 0x50 0x50 0x20 | Data = 41 50 50 20 (hex) |
Rgds
DanS