Hi,
in one of our devices we use the TPS23880 poe chip and configured it to provide a maximum power of 60W (Class 6 and not higher). The connected PD is a camera that requires a maximum power
of 50W (inclusive IR and motor) and if the IR and motor are not used, the input power is less than 30W. According to the manufacturer the camera does not support power negotiation via LLDP,
so I thougth that the camera should be classifed as a class 6 PD. But it is always classified as a class 4 PD. The problem is that if IR and/or motor are used, the required power is higher
than the initially specified 30W and the TPS23880 stops providing power.
Is it possible to force the TPS23880 to provide 60W (i.e. to classify the camera as class 6 PD)?
Does the TPS23880 support power negotiation?
Many thanks and best regards
Philipp