Other Parts Discussed in Thread: LM5156
Hi,
I am trying to create SEPIC regulator configuration using LM51561HQPWPRQ1 IC. My input voltage range is 9V to 16V and required output is 9V/300mA.
I have attached 2 simulation circuit with this and only difference between 2 circuit is that MOSFET p/n is different. Intention of simulation is to find the current flowing through inductor and observe voltage across the MOSFET drain and source terminal to choose the appropriate part.
When i try simulation with 16V input, output is same for both circuit and no anomaly is observed. But when i try simulation with 9V input, output differs for both circuit. I am seeing significant increase in voltage across drain to source mosfet terminal and higher current flowing through inductor. Like to know why there is change in output significantly as it will affect the selection of the MOSFET and inductor. Also like to know whether increased value observed is a simulation model issue and i can ignore the same.