(1) Table 9-1 lists the maximum Iin_DPM for when the BQ25730 is operating at 800kHz, but what about when it is running at 400kHz using a 4.7uH inductor?
(2) Section 9.5.1.9 of the data sheet shows that the IIN_DPM() register must be written with two consecutive bytes. However, Table 9-7 and the detailed description in section 9.6.6 indicate that it is read only. Which is it?
(3) The IIN_DPM() register seems to follow IIN_HOST() (I'm not using ICO), but with an offset that always makes it greater than IIN_HOST(). How is the DPM mode going to be triggered if the BQ25730 goes into host current limiting before then?