Other Parts Discussed in Thread: LM5148
Hi team,
Our customer is using attached quickstart calculator to calculate the power dissipation of LM25148-Q1. From the calculator Efficiency is calculated as 89.1% and total Pd is calculated as 6.2W. However the sum of Pd of each part is calculated as 5.27W below, which does not match the 6.2W result.
- HSD : 1.7W
- LSD : 1.4W
- Inductor : 0.8W
- IC : 1.11W
- Current sense Resistor : 0.46W (=2mohm * 15.19A^2)
- SUM=5.47W
Could you help check if the calculation is correct and what is the reason for the difference?
Condition:
- HSD : Infineon IAUC60N04S6L039
- LSD : Infineon IAUC100N04S6N022
- Inductor : Panasonic ETQP5MR68YLC
- Output Voltage : 3.3V
- Output Current 15.19A
LM5148-LM25148 Quickstart Calculator_rev3forPCI.zip
Thank you,
Muwei Zheng