Other Parts Discussed in Thread: BQ24040
Hi Team,
Can you please help check the schematic for two BQ29737 in parallel below?
The target system has got two Li-Ion Batteries. Each battery is protected with a single BQ29737. The batteries are then connected in parallel to provide a nominal voltage of 3.5V. There is a single Charger IC type: BQ24040 to charge both batteries.
In the case of an over-discharge situation, both protectors disconnect the batteries from the system. After then activating the charger IC, only one battery gets charged and the other one stays in the over-discharged state.
Coul you help troubleshoot the issue? Thanks in advance.
Regards,
Marvin