Hi,
We are using UCC28C42 floating buck converter to generate 15V output. The input is 3phase but i used single phase only to power this IC and circuit. We are facing problem that once we power ON the circuit the VDD voltage goes on increasing through R4 and R5 and once IC gets input voltage close to 15V which is turn ON voltage of this IC, it immediately gets failed and pin 7 & 5 is showing short or less impedance close to 150 ohm. Even after placing zener of 15V across the pin 7 & 5 also no improvement and IC still failing. we dont observe reference voltage as well. we have removed AC input and used DC input after rectifier of 32V but still similar failure observed, we dont see any output and IC gets failed (Pin 7 & 5 less impedance). Please help to debug and suggest any changes are needed. we have done below changes and tested but no positive result.
We have total 400uF capacitor at the input side, in schematic only 2 is visible.
Also i have tested the demo board of UCC28C42 which has 15V/1A output and after that prepared this schematic.
1- C9, Q2, R23 removed. Same failure
2- R20,D6 removed. same failure
3-C1 changed from 3300pF to 2200pF. same faiure.