Part Number: LM337
Other Parts Discussed in Thread: TPS7A33, LM137
Hello All,
For over 10 years I have been using LM337 and LM329DZ or BZ pair to have a low temperature coefficient regulator ( the circuit shown in every LM337 datasheet ). I need around 5-10mA output current. So I can also use a reference like ref5010 IC I guess. Or maybe a negative regulator with low temperature coefficient.
LM329DZ or BZ is an analog devices component and it is kind of expensive component. I am searching for a new way of having a -10V reference.
I have +15VDC and -15VDC power sources present in my PCB. I also use REF5010 in order to obtain 10V with current boost using a transistor ( for 10V I need around 50mA ).
I do not know why LM329 used in LM337 datasheet, how can I implement a suitable texas instruments reference.
Regards,