Hi
VSEL resistor 23.7K to BP1V5 and 12.1K to AGND
Boost voltage range?
Offset voltage?
Thank
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
VSEL resistor 23.7K to BP1V5 and 12.1K to AGND
Boost voltage range?
Offset voltage?
Thank
On Table 7-17, you can look up the resistor codes for a 12.1k Resistor to Ground and 23.7k to BP1V5
This is
Resistor to Ground Code 5
Resistor Divider Code 3
Divider Code 3
This sets
VOUT_SCALE_LOOP = 0.5V
VOUT_MIN = 0.5V
VOUT_MAX 1.5.
VOUT_COMMAND_offset = 1.05
VOUT_COMMAND_step = 0.01
Resistor to Ground Code 5
This sets VOUT_COMMAND to Offset + 5 x Step = 1.05 + 5 x 0.01 = 1.1V