This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP87562-Q1: Alternative for MPF5024AMMA0ES

Part Number: LP87562-Q1

Hi Team,

Could you pls help recommend alternative for MPF5024AMMA0ES? The requirement are:

buck1,   1.5A 0.8V

buck2,    2.25A 1.8V

buck3.    2.55A 1.1V

buck3.    2.5A 1.1V

Besides, pls recommend alternative for MC33PF8100. Thanks.


Best regards,
Hailiang