This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I'm currently in the process of completing the learning cycle. So far the update status is 05 so I was able to update Qmax. After discharging the batteries from full and waiting 5 hours for relaxation, the update status does not go to 06. The [VOK] was cleared and the [REST] flag was set. I recharged the batteries and attempted a second discharge but noticed that the Ra table is not updating during discharge so it would seem that no resistance measurements are taking place at all. I've tried a C/5 rate and a C/7 rate so far. I'm using 4 Kokam LiPo batteries (3300 mAh/cell, Chem ID: 2049) in a 2S2P configuration, a requirement for my application. I attached the log from my first attempt at the learning cycle which includes the full discharge for resistance updates. Can someone advise on what may be going wrong?
Thanks,
Perry
Hello Perry,
Can you share your .gg file with your configuration information as well as the GPCCHEM report you used to find the chem ID?
Sincerely,
Wyatt Keller
Hello Perry,
I'm glad you were able to get this resolved!
Sincerely,
Wyatt Keller