This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello everyone,
My setup is bq40z60 custom board with 3s Panasonic NCR18650B cells, Charging and discharging works flawlessly.Then I process a learning cycle as described in slua777.pdf. Discharge-rest-charge stage has been completed, Qmax has been updated and Update Status has set to 0x05.
However, Ra tables never get updated while discharging, neither it does in the following rest. I've studied the Ra table update conditions, and it didn't seem they had been violated (RDIS flas was never set).
I attached the log file of my learning cycle below.
Hope for your help!BQ40Z60_learning_cycle_2nd_attempt.rar
hi Michael,
Can you attach your gg file? In looking at your log, Resistance should have been updated. What chem id are you using and how did you identify your chem id? Did you make any changes to trace and downstream resistances?
I would recommend running one more cycle and try to have a constant discharge current. Your current wasn't constant although it was within the recommended c/5 to c/10 rate.
thanks
Onyx
Hello Onyx,
I've attached my gg file (exported before and after Qmax update). My chem ID is 2012 according to bqStudio "Chemistry" value for these cells. I didn't make any changes to mentioned resistances.
I use a resistive load, but it's no problem to make a constant current one.
Best regards,
Michael