Other Parts Discussed in Thread: UCC28782, , UCC5304
Hi,
I want to design a with following specifications:
Input voltage: 30V-200V (if too wide, can be made in two options, 30V - 90V, 80V - 200V)
Output voltage: 5V 6A
Currently, I'm following the UCC28781EVM-053 design. In this design from TI, output is designed 15V-4A.
I tried searching model on WEBENCH® Power Designer, but P/N UCC28781 not support.
Please support and send me new design with output 5V-6A.