Other Parts Discussed in Thread: TPS389006
Hi there,
Customer is working on tps389006-Q1 sequence test.
we found a ACT is pulled down by itself for about 1.5ms, the waveform is shown below.
test condition.
1. if the ACT rising edge is ahead of VDD rising edge
2. the ACT signal is pulled down when the VDD reaches about 3.3V.
As the ACT input signal is also used as other devices enable signal, it results in an abnormal on/off for the other device.
please help to double check if this is a normal operation of tps389006-Q1?
BRs,
Shubiao