Other Parts Discussed in Thread: TPS2546, TPS2547
Hello,
I am looking to do a USB-A Dedicated Charging Port (DCP) and there are some parts from the datasheet that I am unclear on. For our application, we are looking to charge basic USB-A products with shorter cables (less than 3m).
1) Can you use this IC without cable compensation? If so, what do you do with the CS pin? Leave it floating? Connect to GND/VIN?
2) If I want to just do charging, I do not need DM_OUT/DP_OUT, correct? I can just leave them floating?
In the Typical Application section of the datasheet, it mentions that DM_OUT/DP_OUT go to "Host Controller," but I don't understand the purpose of it in this setup because it cannot send/receive data from a host controller in this case. If I want to exclusively do charging, floating the DM_OUT/DP_OUT pins is acceptable, correct?