Hi Expert,
Since output voltage of TPS542A50 is setting by VSET pin, could you provide output tolerance (DC accuracy) for 1.8V and 3.3V application?
Thanks,
Ben
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Assuming 0.1% resistors for VSET , For 1.2V and 5.5V, the accuracy is +/- 1.25% and +/-0.55% respectively.
I will see if I can find additional info.
Hi David,
Did you have data without resistors? Customer use 1% resistor typically.
Regards,
Ben
The resistors are needed on the SREF to VSET to adjust the output voltage.
If the resistors are 1.0%. The 1.2V is +/-2.86% and 5.5V is +/- 0.75%
I understand the request, but we do not have data. The 1.8V accuracy is tighter than the 1.2V