We are designing a DC/DC converter using UC3825B. We need a compensator whose transfer function is given below.
4.096
Gcomp(s) = -----------------------------------
7.92e-6 s^2 + 0.0058 s + 1
Is it possible to implement such a compensator with UC3825B?
Is it possible to set the poles of the compensator to the required places, without setting a pole of the compensator to 0(DC)?
We do not want to have a pole at 0 (DC). How can we implement the required configuration.
Thanks a lot
Best Regards
Aycan UCAR