This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hey guys,
I'm covering the Siemens Motion Control division as an analog FAE. Siemens is looking for a PMIC or power supply for LPDDR5. Do we have a sufficient part/solution here (one part solution preferred)? The expected specs are as follows:
VDD2: 1,065V / ~10A Vin: 12V+-5%
VDD1: 1,8V / ~1A Vin: 1,8V or 3,3 V
VDDQ 0,505V / ~1A Vin: 3,3 V
The given values are a first approx. by Siemens. So please let me also know if there are standard specs for powering LPDDR5.
I'm looking forward to your feedback!
Thanks,
Stefan
Hello SR-MVB Team,
Can you please follow up the below request.
VDD2: 1,065V / ~10A Vin: 12V+-5%
SR-LVB is taking care of the remaining two request.
Thank you,
Regards,
Moheddin.