This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Evaluation to the POL HV Buck

Other Parts Discussed in Thread: TPS40170, LM25116, LM25117, LM5642

Hi Sir

We are evaluating the application as follows 

VIN = 36V (Max), IIN = 10A (Max), VOUT = 15V ~ 24V, IOUT = 20A (Max)

Could you please help to recommend the part suitable for our application?

Any comment is welcome!

Thanks

Regards

Ben