Other Parts Discussed in Thread: TPS62162,
I currently use the TPS62162 and I don't need any external resistor there to set the output voltage to 3V3.
When looking at the datasheet of the TPS62901 as an alternative part (due to bad availability of the 62162) it is not completely clear to me, wether or not this same configuration is possible.
It seems to me like I bascially have two options:
1) Connect MODE/S-CONF Pin directly to GND to activate AEE. In this case the output voltage is set with a voltage divider at the FB pin --> two external resistors needed
2) Alternatively I can leave the FB/VSET pin open to select 3V3 fixed voltage. But in this case I have to connect a resistor to the MODE pin to set the mode to fixed voltage operation, correct?
What would happen if I connect MODE to GND and leave the FB/VSET pin open? Is that an undefined operation mode?
Best regards
Julian