Hi Team,
I have query regarding UCC28C56EVM-066. In the data sheet transformer temperature VS Load graph increase in temperature load current need to change but voltage is varying.
Kindly, May I know what the reason for it.
Thank You,
Suma D
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
I have query regarding UCC28C56EVM-066. In the data sheet transformer temperature VS Load graph increase in temperature load current need to change but voltage is varying.
Kindly, May I know what the reason for it.
Thank You,
Suma D
Hi Suma,
I don't understand your question.
This graph shows temperature (y-axis) versus load current (x-axis) with Vin held constant at 200, 400,...,1000V. The load is varying, from <0.25A to 2.75A at each input voltage.
Usually, applications have a typical input voltage, like 800V. So this would correspond to the aqua colored curve.
Regards,
Eric