Hi,
we would like to replace LM2670-ADJ (Vout=15V) bye fixed Output alternatives from the LM2670.
IIf this is possilbe, which resistor setting would you recommended?
Me examples are calculated for the LM2670-12 to set the output voltage to 15V.
Option 1:
Adding a resistor between Output and feedback with 6,1kΩ.
Option 2:
Adding following voltage devider:
Rhigh:10kΩ
Rlow:39k2Ω
BR,
Florian