Hi Sir,
I am a bit confused about choosing capacitors for a very stable voltage reference using REF5020.
Let's look at the following figure
As what I read in the REF50XX datasheet, the output capacitor (the 47uF capacitor in the Fig.10.1) must be a low ESR one, and the total resistor value in series with this capacitor should be from 1Ohm to 1.5Ohm.
There are some more capacitors in the circuit, so is there any similar requirements with those capacitors (the input capacitor at Vin pin, the 10uF ouput capacitor and the 1uF capacitor at the TRIM/NR pin)?
I think the best choice for the 47uF output capacitor is an ultra low ESR tantalum capacitor in series with a 1Ohm resistor. But I am not sure about the others. Am I right?
And can I connect some .1uF NPO capacitors in parallel with the output for getting rid of high frequency spikes?
I am looking for your help.
Thank you and best regards,
Tuan Tran.